SPONSORED
Hardwired or Wireless? Why Not Both?
Meet the Wireless Technology That’s Setting the Standard in Commercial and Residential Security
By Johnson Controls | December 19, 2023
Read Time: 3 Minutes
Getting your customer the right solution means evolving to meet needs as they are uncovered. In the security space, it can take time for integrators to make significant changes like “going wireless,” as a hardwired system may not provide everything the customer is looking for.
Residential and commercial security installers began branching out into the smart-security territory, and the industry needed to adapt, while hardwired installers began to transition into installing full wireless systems. Automation devices like locks, lights, and sockets began to deliver control that was almost unimaginable just a few years before. As these new wireless technologies were developed, two things were at the forefront of research and development throughout the industry: range and security.
Range, which refers to the reach of the signal when traveling long distances, as well as signal strength through thick brick walls or throughout warehouse spaces that are filled with racks of product.
Security, which refers to layers of protection for connected devices, like two-way encryption.
Many hardwired fans have been reluctant to work with wireless peripherals due to lack of signal strength and reliability, oftentimes with good reason. Any device that is not encrypted runs the risk of being hacked and adding a wireless module into a hardwired system will come at a cost.
What are the main differences between a hardwired security system and a wireless system?
Hardwired System Benefits
For many in the security industry, hardwired works better in larger commercial spaces because range isn’t an issue. If a sensor is 5,000 feet away from a central panel, you just need a cable long enough to reach. Hardwired systems also offer reliability where a sensor will only go offline is if the cable is cut or it breaks. Hardwired sensors are also known to be less prone to false alarms due to a low battery or from wireless interference. While hardwired door sensors may be less expensive than a wireless sensor, the price of a wireless sensor can be leveled as it eliminates the cost of cables connecting back to the panel.
Wireless System Benefits
The main benefits to wireless security peripherals are time to install, and overall cost. A wireless sensor can be programmed right next to the panel, and physically installed on any door or window, making it a highly efficient process. The distance between sensors and panels can vary between product lines, but with PowerG wireless technology, range is no longer an issue.
What Is PowerG?
PowerG is a groundbreaking propriety wireless technology that increases security and signal range for wireless security, safety, and automation devices. Supported by powerful features like 128-bit AES encryption, frequency hopping, and 4x the range of legacy wireless protocols, PowerG helps customers create effective, flexible wireless security systems. PowerG signal can travel up to 6,000 feet (line of sight) from our panels without the need for repeaters.
Can you run both hardwired and wireless?
In 2023, Johnson Controls launched the IQ Pro, the first all-in-one hardwired and wireless hybrid panel. The IQ Pro allows hardwired installers to test adding wireless peripherals, while maintaining their typical installation process. We didn’t just add a wireless option, we added PowerG.
ABOUT THE SPONSOR
This article was brought to you in partnership with Johnson Controls.
For nearly 140 years, Johnson Controls has been creating safe, healthy and sustainable spaces with their award-winning digital technologies and services. Through AI and data driven solutions, they’re delivering the blueprint of the future for smart buildings, including healthcare facilities, schools, data centers, airports, stadiums, hotels, and manufacturing plants.