SPONSORED
Unified Industrial Control Solutions Boost Efficiency and Uptime
By Eaton | June 3, 2026
Read Time: 4 Minutes
Connecting powerful, yet disparate components into a unified, scalable solution can improve the performance of packaging lines, pump skids, conveyors and other industrial systems. Together, Wesco and Eaton offer unified industrial control solutions that optimize the operation of OEM machinery and industrial equipment used in data centers, material handling, HVAC, battery manufacturing and other sectors.
A cohesive ecosystem can be used to build repeatable architectures and pair devices with digital tools to solve real-world application challenges. Eaton explains how intelligent protection, motion and control components are combined to create connected, digitalized solutions that simplify commissioning and integration, maximize safety and efficiency, and minimize downtime.
Question 1: With the onboard processing power of today’s devices, how much decision-making occurs at the edge versus in the cloud?
Eaton: Decision making can be divided into three buckets: Primary control (device level), secondary control (supervisory or cell level) and tertiary control (enterprise or cloud level).
Safety-critical or time-sensitive functions — such as speed loops, trips or interlocks that must execute with latencies of micro to milliseconds — are kept at the device level. For example, Eaton’s PowerXL DM1 Pro variable frequency drive (VFD) can regulate motor speed and torque, our Power Defense molded case circuit breaker (MCCB with PXR trip unit) might trip on a fault, or our easyE4 nano programmable logic controller (PLC) can enforce machine interlocks at the device level.
Secondary control coordinates optimization across machines or cells. For example, our XC-303 modular PLC can orchestrate multiple drives on a conveyor line or manage distributed I/O for a packaging system at the supervisory level, while remaining close to the process for fast response.
Cloud control is used for fleet analytics, trend detection, remote diagnostics and functions that don’t have a critical time component. For example, the Brightlayer Machinery Suite can provide predictive insights and energy dashboards across an entire OEM fleet.
Question 2: Can you discuss a scenario where commissioning and monitoring drives remotely via Bluetooth improves safety or reduces downtime?
Eaton: The value is gaining access without unnecessary exposure. Two great examples of Eaton Bluetooth-enabled capabilities support this. Our Power Xpert inControl software for PowerXL VFDs and our S711 Connect app for the S711 soft starter offer Bluetooth connectivity so technicians can pair, parameterize and monitor devices from outside enclosures or away from machines.
The ability to get diagnostics, troubleshoot fault codes or trend motor data without opening the panel reduces the degree to which teams need to power down, lock out and suit up to troubleshoot a pump in a hard-to-reach location, enhancing safety while reducing downtime.
Another time saver is the ability to use those tools to upload, download and distribute parameter sets. Users can connect over Bluetooth and export a parameter set from one unit and use it to set up multiple units in a fraction of the time with fewer errors and less exposure.
Question 3: Can you describe an application where multiple drives are directly controlled and explain the required integration?
Eaton: In a pumping application, a complete solution built from the same product family allows users to scale based on the complexity and size of the application.
In a small pump bank, drives with built-in multi-pump functions or onboard logic can control multiple units without an external PLC. For example, the PowerXL DG1 can act as the lead controller in a multi-pump set, handling speed references, lead/lag and lead-role rotation without an external PLC, making it ideal for booster pumps, pump skids or HVAC banks where simplicity is key.
You can also do this via the onboard Power Xpert inControl Logic Editor, available with our PowerXL VFDs, which uses standard PLC languages, allowing users to build custom sequences, leverage drive I/O, and handle start/stop logic and speed and torque references within the drive.
For complex coordination, the easyE4 nano or an XC-303 PLC can manage multiple drives over Modbus RTU or Modbus TCP, adding flexibility and scalability. For higher performance coordination, the PowerXL DX1 VFD provides advanced control and communications suitable for coordinated multi-drive applications.
Question 4: In a standalone pump station with breakers, drives, PLCs, and an HMI, how important is a seamless communication architecture? Are there advantages to keeping the ecosystem within the same supplier portfolio?
Eaton: When building a pump skid, communication considerations are critical. Many OEMs use Modbus RTU for simplicity, but Modbus TCP or EtherNet/IP can provide Ethernet-based access and broader data sets for diagnostics and remote monitoring via gateways.
In the context of a unified solution, the PLC handles the set points and permissives, the HMI provides visibility and operator interface, the drive shares speed and torque data and provides motor control, and the breaker pushes metering and trip data back into the system. Keeping devices within a compatible portfolio helps ensure built-in protocol support and reduces custom integration.
The copy and paste simplicity of an ecosystem solution allows consistent tag naming, unified software tools and accessories that work seamlessly together, saving time, reducing protocol driver work and streamlining support.
Question 5: How can organizations know which solution is best for them?
Eaton: Every organization is unique, so it’s vital to have a partner who understands your business and its challenges. That’s why we collaborate with Wesco.
Wesco’s automation and control engineering specialists amplify the impact of Eaton’s unified control solutions. These specialists offer deep product competency, real-world application insight and local support to give OEMs direct access to knowledgeable partners who understand their applications and can translate Eaton’s technologies into cohesive, optimized systems that elevate performance, safety and efficiency.
This article was originally published by Control Design. Reprinted with permission of the publisher.
ABOUT THE SPONSOR
This article was brought to you in partnership with Eaton.
Eaton manufactures energy efficient products and services that help customers effectively manage electrical, hydraulic and mechanical power. Capitalizing on the global growth trends of electrification and digitalization, Eaton has committed to helping customers manage power today and well into the future.