Video conference room meeting



SPONSORED

USB-C: The New Standard for Meeting Rooms and Classrooms


The constant struggle with cables, adapters and proprietary systems has transformed simple meetings into frustrating exercises in setup and troubleshooting. Today’s users expect the same seamless “plug-in and go” experience they enjoy at their desks, yet many shared spaces remain hampered by outdated A/V designs that require special instructions or an IT intervention.

Enter USB-C: a single, reversible port capable of delivering power, high-speed data, video, Ethernet and device charging all at once. With USB-C, conference rooms and lecture halls can finally mirror the effortless connectivity of personal workstations.

USB-C as the All-In-One Solution

Regulatory moves like the EU’s common-charger mandate and Apple’s adoption of USB-C on mobile devices have cemented it as the de facto standard for modern technology. For A/V integrators and IT managers, USB-C means fewer cables to manage, fewer compatibility headaches, and a straightforward path to future-proof installations. One small connector now handles power delivery, video transmission, network backhaul, USB-peripheral connectivity, and device charging over a single cable.

USB-C Empowers Bring-Your-Own-Meeting (BYOM)

Bring-Your-Own-Meeting (BYOM) puts the user in control. Instead of fixed room consoles or scavenging for adapters, presenters simply connect their laptop or tablet via USB-C and instantly access displays, cameras, microphones, speakers and network resources. This user-centric approach slashes setup time, eliminates compatibility headaches, and ensures every meeting—whether on Zoom, Teams or Google Meet—flows smoothly. Educators can move fluidly between venues without relearning A/V systems, and corporate teams can collaborate without delays or support tickets interrupting their workflow.

Future-Ready Workspaces Centered Around USB-C

As organizations build their next-generation facilities, they’re investing in automated room controls that anticipate meeting setups, AI-powered cameras and microphones that enhance equity for remote participants, and modular connectivity hubs driven by USB-C simplicity. Standardizing on USB-C lays the foundation for faster installations, painless upgrades, and a truly frictionless user experience.

The Technical Edge of USB-C in A/V and the Challenges It Presents

The technical advantages of USB-C in A/V are profound. A single cable handles video, audio, USB peripherals, network access, and power delivery, massively reducing clutter and confusion. Its support for multi-display configurations through standards like DisplayLink and DP-MST lets users enjoy dual screens on both PCs and Macs without extra dongles or complex settings.

However, USB signals are natively limited to very short distances, and the USB devices are designed to be directly connected to a single host computer. This makes using USB-C in conference and learning spaces a challenge where users need USB devices such as cameras and microphones to be placed in distant locations around the room. Switching these devices and providing connectivity for multiple laptops and connectivity types is also a regular expectation and is equally a major challenge.

Introducing the Liberty TeamUp+ Series TU-DS42 Multiscreen BYOM Switcher and Extender

Building on this USB-C revolution, the Liberty TeamUp+ Series delivers a ruggedized, pro-grade tabletop solution built for constant use in commercial settings. The TU-DS42U3-H3 switcher consolidates video, audio (analog and Dante), USB 3.0, Ethernet and power over one USB-C cable. It automatically routes signals to both the room’s displays and its cameras, microphones and speakers. Its companion receivers, the TU-DS42U3-RX and TU-DS42-RX, extend those connections up to 100 meters and provide additional USB ports and a second display output wherever they’re needed. Built-in DP-MST and DisplayLink offer native multiscreen extension, performing just like the user’s personal workstation.


Liberty TU-DS42U3-H3 Switcher Liberty TU-DS42U3-H3 Switcher

By eliminating dongles, adapters and guesswork, TeamUp+ DS42 brings the familiarity of a personal workspace to every shared environment. It ensures that walking into a room and plugging in is all it takes to start a productive, professional A/V experience.

Looking Ahead

As the A/V industry shifts toward simplified, user-driven designs, USB-C stands at the forefront of that transformation. Solutions like the Liberty TeamUp+ DS42 Series not only solve today’s connectivity headaches but also pave the way for adaptable, future-ready installations.



Woman holding hybrid conference near screens

Upgrade your Meeting Rooms and Classrooms with Liberty A/V Solutions



 

ABOUT THE SPONSOR

This article was brought to you in partnership with Liberty.
Liberty provides a comprehensive technology ecosystem of innovative, advanced infrastructure systems for pro A/V, security and surveillance, cable and connectivity, wireless, and distributed antenna systems trusted by integrators worldwide. From design assistance and kitting to global logistics and training, Liberty empowers partners to create connected, secure and future-ready environments.


You might also like