CASE STUDY
How Wesco helps standardize complex security rollouts
Challenge: Inconsistent deployments slowed multi-site execution
A leading security integrator was supporting a large self-storage provider that required camera, NVR, and encoder configurations across a broad network of sites. The integrator was struggling to perform the required configurations at the scale and pace needed, which caused the program to fall behind schedule. In some regions, work had to be outsourced to third-party installers, creating inconsistency in how deployments were completed.
This issue created several operational concerns. In some cases, onsite teams were not following installation standards, using cameras that did not meet approved specifications or failing to complete device configurations correctly. This resulted in rework, inconsistent site readiness and growing complexity across the customer’s environment. Because individual facility operators were sometimes sourcing devices independently, the end customer was also facing a fragmented camera landscape with systems that did not always align to enterprise standards or integrate properly across the broader platform.
The program was also being impacted by lost onsite deliveries and product availability challenges. Multiple shipments arriving without enough coordination made it difficult to maintain visibility and control at the site level, while stock constraints were pushing completion schedules further out. As a result, the integrator needed a scalable, controlled and standardized delivery model to regain consistency, improve execution and meet customer expectations.
Project Summary
- Challenge: Inconsistent multi-site deployments and supply delays
- Solution: Centralized kitting, standardized processes and inventory planning
- Results: Greater deployment consistency, visibility and on-time completion
Solution: Centralized support created repeatable deployment control
Wesco supported the project with kitting and installation enhancement services, helping create a more scalable and repeatable deployment model. The work was centralized through a Wesco Technology Deployment Center, improving consistency across the program and giving the integrator a more reliable delivery engine.
To improve field execution, Wesco included a technician completion checklist in each shipment so onsite teams could complete work according to defined deployment standards. Wesco also began kitting all materials going to each site into clearly identified shipments, with exterior labeling that indicated the purpose of the material. Prior to shipment, the integrator was notified so it could schedule technicians and alert site personnel in advance. This improved communication, reduced confusion around multiple deliveries, and created stronger control over materials from shipment through installation.
To address product availability issues, Wesco proposed quarterly stock buys and pre-provisioned 90 days of material up front. This helped avoid stock-outs, supported better continuity across the rollout, and kept projects moving on schedule.
Results: Improved consistency helped restore customer confidence
With Wesco’s support, the integrator was able to scale more effectively, improve deployment consistency, and better meet the expectations of its end customer. The partnership helped stabilize a program that had been falling behind and enabled the integrator to retain a strategic account that had been at risk due to inconsistent execution.
The updated delivery model gave the integrator stronger chain of custody over materials, eliminated lost shipments onsite and helped work get completed by the expected deadlines. Standardized kits, clearer communication, and better field controls reduced variation across locations, while advance inventory planning eliminated stock-outs and kept the rollout moving.
Ready to simplify complex security deployments?
Connect with Wesco to learn how our kitting, logistics and deployment support services can help improve consistency, control and scalability across your next rollout.