SPONSORED
Architecting Resilient Data Center Networks to Meet AI Demands
By Siemon | January 28, 2026
Read Time: 3 Minutes
Artificial intelligence (AI) and machine learning (ML) workloads are reshaping the digital infrastructure landscape, driving demand for faster, more scalable and more resilient data center networks. Traditional architectures are no longer sufficient to support modern requirements. A dual‑network design, optimized for both general‑purpose computing and high‑performance computing (HPC), helps meet ai data center networking demands like training, inference and large‑scale data movement, with verified performance and future‑ready scalability.
Bridging the AI Divide with Dual-Network Architecture
Modern data centers increasingly rely on two distinct but interconnected networks:
Front-End Network
This is a general-purpose infrastructure supporting central processing unit (CPU) servers, storage and north-south traffic. Typical designs use spine-leaf cabling topologies with 200/400G Ethernet switch-to-switch links and 25/50/100G switch-to-server connections.
Back-End Network
Purpose-built for AI and HPC workloads, this closed spine-leaf topology facilitates east-west traffic across graphic processing unit (GPU) clusters. These environments demand ultra-high-speed interconnects, such as 800G Ethernet and InfiniBand™, and are preparing for 1.6T technologies.
Trusted partner solutions seamlessly integrate these networks, whether deployed in edge AI racks, experimental pods or hyperscale environments.
Siemon AOC 1xQSFPDD 2xQSFPDD
Siemon BASE8 MTP TRUNK Green Blue
Siemon DAC Cable
Optimizing Interconnection Performance
High-performance interconnection spans four critical areas of AI data center networking:
Front-End Switch-to-Switch
Direct attach copper (DAC), active optical cables (AOC) and BASE-8 MTP cabling support 200G and 400G Ethernet links. Breakout configurations (e.g., 2x200G, 4x100G) enhance port utilization and space efficiency.
Front-End Switch-to-Server
LC/MTP jumpers, Cat6/6A small patch cords, DACs and AOCs support 25G, 50G and 100G server links across ToR, MoR and EoR topologies.
Back-End Switch-to-Switch
For HPC environments, 800G Ethernet connectivity using DACs, ACCs/AECs and BASE-8 MTP cabling support both row-to-row and within-row deployments.
Back-End Switch-to-Node
AI pods typically utilize 400G to 800G GPU connections to leaf switches. CPU nodes connect to the front-end network at 100G, with copper links supporting out-of-band management. Connectivity options vary by required length and reach.
Siemon Cabling Map and Suggested Link Length
Cabling Topologies That Scale with AI
Siemon’s broad portfolio supports both point-to-point and structured fiber systems, enabling flexible cross-connects and simplified upgrades. Breakout configurations maximize port density and space efficiency, while ToR, MoR and EoR layouts adapt to rack density, cooling needs and latency requirements.
Featured solutions include:
LightVerse® Fiber System: Ultra-low-loss MTP-to-LC modules for 800G+ applications
LightStack® High-Density System: Supports up to 864 MTP fibers per rack unit
High-Speed Cable Assemblies: DACs, AOCs, ACCs/AECs available in multiple lengths and breakout options for Ethernet and InfiniBand™
Building the Future of AI Data Center Networking
As AI workloads continue to accelerate, Siemon is committed to helping customers architect resilient, scalable and high-performance environments. Through strategic partnerships and a robust mix of copper, fiber and high-speed connectivity, organizations can confidently support evolving AI and HPC demands.
ABOUT THE SPONSOR
This article was brought to you in partnership with Siemon.
Siemon is a global market leader in the design and manufacture of high-performance connectivity solutions for data centers and smart buildings. The company empowers customers to connect faster, scale smarter and deploy with confidence. With operations in over 100 countries, Siemon is the trusted partner behind the networks that connect the world.