- Facility Perimeters
- Facility Exteriors
- Common Areas
- Interior Areas
- High Security Areas
SPONSORED
By dormakaba | October 8, 2025
Read Time: 3 Minutes
The global data center market continues to grow, becoming a key point of global connectivity. Unauthorized access, human errors, theft and protocol failures can create vulnerabilities within a center. Protecting these hubs is no longer optional; it is essential for operational integrity and customer trust. Each facility has a unique layout, operational needs and threat landscape – there is no universal solution.
A layered approach to physical security is crucial for safeguarding data centers from the outside in. From the perimeter to high-security interior zones, thoughtful planning builds a resilient security posture. In this article, we will break down the five primary layers of physical security in a data center:
Source: dormakaba
A secure data center begins at its perimeter, making the fence line a vital first layer of defense. It serves as the initial checkpoint where all visitors are vetted before gaining access to the facility. Strategically placed guard booths with credential readers manage automated vehicle gates, while full-height turnstiles secure pedestrian access. These physical access points integrate with a facility’s broader access control system, supporting proximity card or biometric verification. In addition to entry control, the perimeter also safeguards exterior utility areas – often vital to operations – ensuring comprehensive protection. Together, these measures create a seamless, efficient and resilient approach to physical security.
Exterior data center entrances are key transition points where visitors enter the facility. Standardized interlock portals help control access by supporting dual authentication, such as proximity cards and biometrics, ensuring only authorized personnel enter. Metal detection at these entrances adds security by preventing unauthorized data storage devices or restricted tools from being brought inside.
Combining these technologies helps facilities maintain strict access protocols while offering an efficient, professional experience for personnel and visitors.
More than welcoming spaces, lobbies and reception areas are essential for managing movement within a data center. These common areas guide visitors and personnel to authorized destinations while offering secure checkout stations to reduce the need for outside tools. Interior full-height and optical turnstiles add a layer of verification before individuals reach sensitive areas. Optical turnstiles at elevator banks, paired with elevator dispatch features, help ensure access is limited to approved floors based on credentials. These systems support a secure, efficient and controlled flow throughout the facility’s most active shared spaces.
Interior areas such as offices and break rooms are essential to daily operations, but often contain sensitive information and department-specific resources, so access must be restricted to authorized personnel. High security door locks with credential readers tied to the building’s access control system help to ensure only authorized individuals can enter. It is common practice for staff to have access only to offices within their assigned department, minimizing unnecessary exposure. This targeted approach not only protects critical assets but also supports operational efficiency and reinforces consistent, role- based access control throughout the data center.
High security areas such as server and utility rooms require the most robust physical protection, as they house essential infrastructure and sensitive data. True preventative measures are necessary for detecting unauthorized access like tailgating or piggybacking and stopping it entirely. Interlock portals and security revolving doors offer controlled, single-person entry with authentication verification. Server rack locks add another layer of defense, securing access to equipment within the room itself. By working in tandem, these solutions ensure only authorized individuals gain entry, reinforcing a strong, layered security strategy across the facility’s most critical zones. Additionally, each data cabinet should have access control designed into the front and back cabinet doors and should monitor the cabinets for door propping and latching.
A layered approach is essential for maximizing a data center’s security. As a mission-critical factor in data center operations, incorporating physical security design during the design process offers the most cost-effective solution, the best use of technology and most effective facility integration. Designing access control at every layer, being aware and following the protocols are key to effective security protocols. Each component and access point builds on the other to create a resilient security posture.
ABOUT THE AUTHOR
This article was brought to you in partnership with dormakaba.
Rick Estes is the Associate Vice President of Business Development at dormakaba North America. He has been with dormakaba for 14 years and has over 35 years of experience in the security and door hardware business.