SPONSORED
Enterprise A/V Performance with Intelligent PDUs
Elevate your power strategy and optimize your A/V infrastructure
By Legrand | AV | November 13, 2025
Read Time: 4 Minutes
Audio/video (A/V) professionals recognize that power conditioners and filters are essential to provide a clean, consistent power supply necessary for reliable A/V performance. However, power conditioners are only part of the solution.
In the enterprise environment, A/V administrators require a power strategy that ensures control centers, broadcast rooms and enterprise A/V systems are resilient and performing optimally. Key to this strategy are intelligent power distribution units (PDUs) and innovative cable management solutions.
Why Power Matters for Enterprise A/V Systems
Imagine this: digital signage at a retailer’s flagship store suddenly goes dark. A conference call with a key client is disrupted by video jitter and lag delays. Audio during a live event becomes distorted. These are nightmare situations for teams responsible for enterprise A/V installations. Organizations today rely on seamless multimedia experiences as part of their day-to-day operations to drive productivity, customer satisfaction and revenue.
Any number of issues can cause A/V difficulties, but poor power quality is often the root cause. Clean electrical power is essential for all electronic equipment, particularly high-fidelity A/V systems. Even minor power inconsistencies can introduce perceptible noise, distortion or downtime.
What Are Intelligent PDUs?
Intelligent PDUs do more than deliver clean power. They provide the visibility, automation and control needed to maximize uptime and ensure a high-quality user experience. Network-connected smart PDUs allow operators to:
- Monitor power quality and usage in real time
- Remotely manage power delivery down to the outlet level
- Set thresholds and receive alerts for critical loads
- Identify underperforming equipment and optimize capacity planning
This means you can spot issues before they become problems, prevent unnecessary power usage and ensure every device is running at peak efficiency.
Remotely Monitor Real-Time Power Metrics
Metering is a core capability of intelligent PDUs. Integrated sensors capture power metrics at various points, including the PDU inlet, individual branch circuits and each outlet. Operators can remotely view power usage in real time, helping them understand current loads and capacity.
Operators can set thresholds at various levels of granularity, such as the overall unit, individual circuits and individual outlets. The intelligent PDU can then issue an alarm if the power draw reaches a critical level or a warning if a device approaches a critical load. This alert allows operators to take quick action to prevent a tripped breaker or damage to equipment.
By monitoring power consumption, operators can identify equipment that is consuming less power than expected, which could indicate a problem or underutilization. Monitoring also helps prevent unnecessary power usage, facilitates capacity planning and optimizes the use of space.
Remotely Control Individual Power Outlets
Some intelligent PDUs allow individual outlets to be switched on and off remotely for troubleshooting or power scheduling. In many cases, turning equipment off and on is all that’s needed to resolve problems. The ability to power cycle equipment remotely eliminates the need for a technician to visit the site to perform this simple task.
Staged power sequencing is especially important in A/V systems where components must power up in a specific order to protect sensitive equipment. Sequencing helps prevent voltage spikes during power up, which could be sent through the system and potentially damage speakers or create a power surge that trips circuit breakers. Because A/V systems often rely on a specific order of operation to function correctly, intelligent PDUs can automate the power sequencing process for one-button simplicity and reduce the risk of human error.
A/V operators can also use switched PDUs to improve power management. Running noncritical equipment when it’s not needed wastes electricity and increases costs. Switched PDUs enable operators to control power on a per-outlet basis, allowing for precise power management.
Why A/V Installations Need A/V-Specific PDUs
Many data centers utilize intelligent PDUs to ensure reliable power for equipment, facilitate remote operations and meet sustainability goals. These benefits translate to A/V use cases like managing digital signage networks, classrooms, conference rooms, and other large-scale and distributed spaces.
However, when planning power for environments with more unique A/V needs – professional installations, studios, broadcast facilities, live events – operators should choose PDUs designed to:
- Clean, filter and stabilize power for sensitive A/V equipment
- Provide multi-stage surge protection and active voltage regulation
- Enable precise power sequencing to protect speakers and amplifiers
Best-in-class A/V-specific PDUs deliver these advanced features, reducing susceptibility to power fluctuations and protecting your systems against performance degradation and damage.
The Importance of Effective Cable Management
Proper cable routing is essential for preventing electromagnetic interference (EMI) and maintaining signal integrity. Because power cables carry significant electrical current that produces electromagnetic fields, power cords and A/V signal cables should be routed along separate pathways to minimize audio hums or video signal degradation. Careful cable routing and isolating metal components also help prevent “ground loops” that can cause unwanted noise.
Right sizing your cable is also a crucial factor in cable management. Over long runs, it’s important to consider voltage drop, where power is lost due to the resistance of the wire along its length. Tightly coiling extra cable can create an antenna-like effect, increasing the potential for both picking up and radiating noise. Using the correct size and length of cable for your application is key for reliable performance of your A/V system.
Effective cable management also improves airflow. Cluttered, bundled cables can obstruct airflow, leading to equipment overheating. Higher temperatures can increase electrical resistance in wires, contributing to voltage drop and potentially shortening the lifespan of components.
High-quality A/V mounting systems include integrated cable management for a professional installation. These systems work in conjunction with intelligent PDUs to create a comprehensive power strategy.
Wesco: Expert Guidance for Scalable A/V Solutions
Ignoring power quality comes at a significant cost. Voltage fluctuations and surges can significantly reduce the lifespan of electronics. “Dirty power” can prevent A/V equipment from operating at its peak, resulting in a degraded end-user experience. In a commercial setting, equipment malfunction due to poor power can hinder productivity and lead to expensive service calls and lost business.
Wesco’s A/V experts can help you develop an intelligent power strategy that uses advanced technology and data analysis to deliver electricity more efficiently, reliably and sustainably. We’ve partnered with Legrand | AV to offer intelligent PDUs that provide remote monitoring, control and environmental sensing to protect your A/V equipment.
ABOUT THE SPONSOR
This article was brought to you in partnership with Legrand | AV
Legrand improves lives by transforming the spaces where people live, work and meet, with electrical and digital infrastructure and connected solutions that are simple, innovative and sustainable. Its comprehensive offering of solutions for commercial, industrial and residential markets makes it a benchmark for customers worldwide.