ARTICLE
Leveraging Commercial Battery Storage Systems To Drive Results
Why Battery Energy Storage Systems are on the Rise for Commercial Facilities
By Jesse Vanderhoof | June 12, 2026
Read Time: 3 Minutes
Battery energy storage systems (BESS) have become essential infrastructure for commercial facilities in 2026. As utilities modernize grids and demand charges continue to rise, businesses are increasingly adopting energy storage to improve operational resilience, reduce energy expenses and participate in profitable grid services programs. Updated state programs have expanded commercial incentives and performance payments, accelerating adoption across sectors.
Four Top Reasons To Adopt Commercial Battery Storage Systems
Major Cost Savings Through Demand Charge Management
Commercial buildings face high demand charges, and BESS helps lower these costs by shifting energy use. By charging during off-peak hours and discharging during peak periods, BESS reduces the building’s maximum demand, a key driver of electricity bills.
Beyond peak shaving, BESS can support demand response by reacting to utility signals or pricing, further cutting costs and potentially generating revenue. When paired with on-site solar, it stores excess daytime energy for use during high-cost periods, improving self-consumption, reducing grid reliance, and enhancing overall resilience.
Improved Operational Resilience for Critical Facilities
Facilities depend on continuous power, and BESS plays a critical role in responding to outages in real time. When a grid disruption occurs, the battery system can instantly discharge, providing seamless, uninterrupted power to critical loads without the delay associated with generators starting up.
BESS can also be configured to prioritize essential equipment, ensuring that the most critical systems remain operational during an outage. For grid-edge customers, who often experience longer or more frequent outages, this rapid response capability is especially valuable, reducing downtime, maintaining safety and improving overall resilience until grid service is restored or other backup systems take over.
Participation in Grid Services and New Revenue Streams
Commercial battery storage systems enable businesses to turn energy assets into ongoing revenue opportunities. By enrolling in grid services programs, facilities can dispatch stored energy during summer and winter peak demand events, when the grid needs support most. In return, utilities provide recurring performance incentives over multi-year terms. These programs improve return on investment while helping strengthen grid reliability and resilience.
Access to Incentives and Accelerated Deployment
Commercial energy storage adoption is accelerating thanks to incentive structures designed to reward early participation and strategic grid placement. Declining block incentives provide higher upfront payments to early adopters, encouraging faster deployment of battery systems while still offering meaningful savings as programs mature. Grid-edge adders further increase incentives for facilities located in areas with higher outage risk for grid congestion, where energy storage delivers the greatest reliability and grid support value. The Federal Investment Tax Credit (ITC) provides a 30% credit for storage through 2033, with adders enabling up to 50% savings.1
In addition, expanded capacity allocations set aside more megawatts specifically for commercial customers, helping to ensure greater program access as demand grows. Recent updates reduced commercial incentive levels amid high demand while expanding overall program capacity.
Together, these mechanisms help reduce upfront costs, improve project economics and accelerate time to deployment.
Why Wesco for Commercial Battery Storage Systems
Wesco provides end-to-end battery energy storage solutions for commercial customers seeking greater efficiency, cost savings and resiliency. Because every building has unique usage patterns, utility rate structures, regulations and incentive opportunities, BESS projects require a customized approach. Wesco supports customers through design, engineering, system optimization, financial and feasibility analysis, sourcing, logistics, commissioning, and technical support for projects ranging from 20 kWh to 20 MWh. Backed by strategic supplier partnerships and expertise in distributed energy, EV infrastructure, controls and microgrid integration, Wesco delivers the reliable solutions and trusted guidance businesses need to deploy energy storage with confidence.
ABOUT THE AUTHOR
Jesse Vanderhoof
Senior Director, Sales
Jesse Vanderhoof is an industry leader in solar and renewable energy with over two decades of experience driving growth, building strategic partnerships and scaling high-performing teams. As Senior Director, Sales at Wesco, Jesse focuses on accelerating the adoption of solar, storage and electrification solutions across commercial, residential and utility markets.