SPONSORED
Mobile-Enabled Electronic Locks for Multifamily Properties
Allegion’s modern security solutions offer several benefits for residents and property owners
By Allegion | October 30, 2024
Read Time: 3 Minutes
As the multifamily housing market continues to evolve, property owners are increasingly seeking ways to enhance security, convenience, and overall resident satisfaction. One significant technological advancement gaining traction is the adoption of mobile-enabled electronic locks like the Schlage Control Smart Lock. These modern locking solutions offer a plethora of benefits that make them a worthwhile investment for multifamily property owners.
Enhanced Security
Traditional keys and locks have long been the standard for securing properties, but they come with several vulnerabilities. Keys can be lost, stolen, or duplicated without authorization, posing significant security risks. Mobile-enabled electronic locks, like the Schlage Control, mitigate these issues by utilizing digital keys that can be managed and monitored remotely. This technology allows property managers to grant or revoke access instantly, reducing the risk of unauthorized entry.
Moreover, mobile-enabled locks often come equipped with advanced encryption and authentication protocols, making them far more secure than their mechanical counterparts. The ability to track access logs also provides an additional layer of security, as property managers can monitor who enters and exits the premises and at what times.
One of the most appealing aspects of mobile-enabled electronic locks is the convenience they offer to both residents and property managers. Residents no longer need to carry physical keys, which can be easily lost or misplaced. Instead, they can use their smartphones to unlock doors, providing a seamless and hassle-free entry experience. This is particularly beneficial in multifamily properties where residents may need to access multiple areas such as the main entrance, individual units, gyms, and other communal spaces.
Schlage Control® Mobile Enabled Smart Lock
Shop now on anixter.com.
For property managers, the ability to manage access remotely is a game-changer. They can issue digital keys to new residents, maintenance staff, or delivery personnel without needing to be physically present. This not only saves time but also streamlines operations, making property management more efficient
Cost-Effective in the Long Run
While the initial investment in mobile-enabled electronic locks may be higher than traditional locks, the long-term benefits often outweigh the costs. The reduction in expenses related to rekeying locks and replacing lost keys can lead to significant savings over time. Additionally, the enhanced security features can lower insurance premiums, further offsetting the initial investment.
Improved Resident Experience
In today’s competitive rental market, providing a superior resident experience is crucial for retaining tenants and attracting new ones. When asked in a recent Multifamily Living Trends Study, nearly 60% of survey respondents stated they would likely select a future place of residence if it had mobile access control offered as an amenity. Compared to the 2019 study, there was an 82% increase in the number of respondents who would be willing to pay more for mobile access control that would allow them to remotely monitor entry of their home and give access to guests and others.
Mobile-enabled electronic locks, like the Schlage Control, contribute to a modern and tech-savvy living environment that appeals to a wide range of residents, particularly tech-savvy millennials and Gen Z renters. The convenience and security offered by these locks can significantly enhance resident satisfaction, leading to higher retention rates and positive word-of-mouth referrals.
Future-Proofing the Property
As technology continues to advance, integrating smart solutions like mobile-enabled electronic locks can future-proof multifamily properties. These systems are often compatible with other smart home devices, allowing for further upgrades and integrations down the line. By investing in such technology, property owners can ensure their properties remain relevant and attractive in an increasingly digital world.
Environmental Benefits
Mobile-enabled electronic locks also offer environmental benefits by reducing the need for physical keys and the associated plastic and metal waste. Additionally, many of these systems are designed to be energy-efficient, further contributing to sustainability efforts.
Stay Ahead of Future Competition
Upgrading to mobile-enabled electronic locks is a strategic move that offers multifamily property owners numerous benefits. From enhanced security and convenience to cost savings and improved resident experience, these advanced locking systems are well worth the investment. As the multifamily housing market continues to embrace technological advancements, property owners who adopt mobile-enabled electronic locks will be well-positioned to meet the demands of modern renters and stay ahead of the competition.
Learn how Allegion and Wesco are creating safer public and commercial spaces.
ABOUT THE SPONSOR
This article was brought to you in partnership with Allegion.
Allegion helps keep people safe and secure where they live, work, and visit. With more than 25 brands sold globally, Allegion specializes in security around the doorway and adjacent area. As a distribution partner, Wesco delivers a full array of Allegion locking and access control solutions to customers around the globe.