University students outdoor walking campus



SPONSORED

Overcome Infrastructure Challenges for Modern Campus Networks


For years, enterprise and campus network managers have worked behind the scenes to keep pace with rapid technological changes. Today, the shift from basic connectivity to immersive, high-performance experience networks is accelerating that challenge. These modern networks must deliver blazing-fast speeds, seamless all-wireless access and application-level performance guarantees.1

To meet these demands, campus and enterprise networks must support true IT/OT convergence and a growing ecosystem of connected devices – including sensors, Wi-Fi access points, DAS, building management systems and more. The result is a network infrastructure that’s hyperconnected, fiber-dense, intelligent and far-reaching. At the same time, speed of deployment, ease of management, security and future scalability are all critical.

Here are some of the key challenges facility and network managers face today:

Extended Reach

As the number of connected devices and systems grows, particularly at the network edge, so does the distance between endpoints and the network core. On large campuses, this can span several kilometers. To bridge that gap, network teams need structured cabling solutions that extend reach while delivering reliable power and data wherever it’s needed.

Rising Bandwidth Demand

More devices mean more data. To keep up with surging bandwidth demand, fiber density is increasing – especially in horizontal access networks. Backbone cabling is shifting from multimode to singlemode, and 100 Gb switches are becoming more common in telecom rooms. To support these higher speeds and densities, many networks are adopting pre-terminated MPOs and trunk assemblies in the backbone.

Redundant Ring Architectures

Ring topologies remain a go-to for campus networks due to their simplicity. But as uptime and reliability metrics become more critical, traditional one-way ring architecture is evolving. Bi-directional links enable the ring to pass traffic in both directions, building in critical redundancy. This approach is also being applied in greenfield facility builds, where dual OSP conduit banks enter buildings from opposite sides to ensure continuity.

Evolving Connectivity Methods

As splicing equipment becomes more affordable, fusion splicing is replacing older, labor-intensive methods like epoxy polish. Even smaller contractors can now use single fusion splicers, while larger contractors are turning to mass fusion splicing with ribbon cables. Fusion splicing with cassettes is preferred over splice-on connectors for its reliability and consistency. At the rack level, LC connectors are giving way to MPOs that connect directly to switches. And most of these connectivity changes are driven largely by bandwidth needs.

Skills Shortage

The global fiber industry continues to face a shortage of skilled technicians. For campus and enterprise network managers, the challenge is even greater. Many experienced techs are moving to higher-paying roles in the data center space, leaving gaps that slow both deployment and ongoing management.

Day 2 Management Costs

As networks grow more complex, so do the costs of managing them. Many teams still rely on manual spreadsheets to document network configurations, an approach that becomes less accurate over time with additions and modifications. Planning upgrades is also costly and time-consuming. Designers often calculate link loss budgets manually to determine whether a new link will support the application performance demands, which can be labor-intensive and still leave uncertainty about whether the network will meet performance requirements.

Conclusion

Your campus network is more than IT infrastructure – it’s a reflection of your organization’s vision and values. Whether you’re building a smart university, medical or corporate campus, you’ll need to address extended reach, rising bandwidth demands, redundancy needs, evolving connectivity, talent shortages and management costs. The right partner can help you navigate these challenges with confidence and help design solutions tailored to your unique requirements.


1Enterprise Networks Evolve From Basic Connectivity to Dynamic Experiences; Light Reading; April 29, 2025



High school students walking in hallway

Learn more about Wesco’s campus solutions for enterprise-grade networks.



 


ABOUT THE SPONSOR

This article was brought to you in partnership with Commscope.
CommScope pushes the boundaries of communications technology to build the world’s most advanced networks. We design, manufacture, install and support the infrastructure and intelligence that power broadband, enterprise and wireless connectivity – solving today’s challenges and driving the innovation that shapes what’s next.



You might also like