Data center aisle futuristic



SPONSORED

Powering the AI Revolution: How Wesco and ABB Accelerate Data Center Deployment

As demand for AI-ready infrastructure surges, strategic partnerships and innovative electrical solutions are redefining speed, reliability and scalability in the data center market.



The surge in AI adoption is fueling an unprecedented demand for data centers – and with it, a race to deploy reliable electrical infrastructure at record speed. Traditional hubs like Northern Virginia and Silicon Valley are facing power constraints, pushing developers toward alternative regions such as Iowa, Nebraska, Nevada, Georgia and Texas, where generation capacity, fiber connectivity and more affordable land are more accessible.

At the same time, the aging electrical grid requires sweeping upgrades and equipment replacements. Lead times for mission-critical components – such as medium-voltage (MV) gear and transformers – can stretch beyond a year, making proactive planning and product availability essential.

This is where strategic partnerships come into play. Wesco, in collaboration with ABB Installation Products, is helping developers, contractors and operators accelerate deployment timelines without compromising safety or reliability.

Adapting Power Distribution Strategies Amid Scarcity

Power availability has become a defining constraint for data center projects. Developers often purchase land and begin construction only to face significant delays in grid power connections. To bridge the gap, some are turning to natural gas generation, while others are shifting builds to regions with more abundant land and power.

This shift underscores the importance of robust medium-voltage systems deployed on-site. ABB Installation Products offers MV solutions up to 38kV and LV solutions up to 1000V, enhancing resiliency and reliability whether owned by the utility or the data center. Through Wesco’s distribution network, these solutions are available when and where they’re needed most.

Balancing Speed, Cost, and Long-Term Performance

As facilities scale to 100 MW or more, infrastructure must support rapid deployment and long-term scalability. ABB’s Elastimold® dead-front solid dielectric switchgear is fully insulated and shielded, reducing arc flash risk and eliminating air, oil or gas exposure – a future-proof solution that is safer, scalable and sustainable.

Wesco ensures these advanced products are accessible through streamlined procurement and inventory strategies, helping contractors avoid delays and meet aggressive timelines.

Designing for Speed and Safety

Every moment of delay in data center construction is costly. ABB’s innovations – such as riveted strut for enhanced cable support and reusable Ty-Grip™ for faster retrofits – are engineered for quick, safe installation. Wesco’s logistics expertise ensures these products are delivered on time, reducing labor risk and accelerating go-live dates.

Overcoming Supply Chain Challenges

Lead times remain a critical challenge. Early engagement with Wesco and ABB allows projects to secure high-quality products during planning stages and maintain inventory readiness. This proactive approach minimizes surprises during installation and keeps projects on schedule.

Efficiency Through Innovation

From Color-Keyed® lugs that prevent installation errors to cable glands that protect against contaminant and moisture ingress, ABB’s solutions prioritize safety and speed. Wesco’s role is to make these innovations readily available, backed by technical support and supply chain reliability.

In today’s fast-paced data center market, speed is the currency – and partnerships are the engine. Wesco and ABB Installation Products deliver the solutions, expertise and availability needed to meet deployment timelines without sacrificing quality or safety. Together, we’re powering the future of AI-ready infrastructure.

Ready to accelerate your next data center project?

Contact your local Wesco representative or visit Wesco.com/abb to learn more about how our partnership with ABB can help you deploy faster, safer and smarter.

 

ABOUT THE SPONSOR

This article was brought to you in partnership with ABB.
ABB is a technology leader in electrification and automation, enabling a more sustainable and resource-efficient future. Building on over 140 years of excellence, ABB is committed to driving innovations that accelerate industrial transformation with solutions that connect engineering know-how and software to optimize how things are manufactured, moved, powered and operated.


You might also like