Simplify the AI Transition With Next-Gen, Modular Fiber Frames



SPONSORED

Simplify the AI Transition With Next-Gen, Modular Fiber Frames


AI has fundamentally changed how data centers are designed, built and managed. Nowhere is this more evident than the fiber infrastructure, where fiber counts now exceed 6,912 in hyperscale environments and reach 1,728 in MTDCs. Network managers know that these escalating fiber counts will eventually affect their enterprise networks, putting pressure on them to scale rapidly with minimal margin for error. Simultaneously adding to this pressure is the fact that compute, storage, power and cooling demands also continue to rise while available space continues to shrink.

A common but critical denominator? The multiple fiber frames throughout the data center. These hubs interconnect and cross connect the backbone, spines/super spines and leaves of the network, distributing capacity to data halls, rows and cabinets. If the frames can’t keep up with the growth, the entire data center risks falling behind.

Network Trends Reshaping Fiber Frame Requirements

Fiber frames are foundational connecting points throughout a data center. As fiber infrastructure and network architectures evolve, the functional requirements of fiber frames must change to keep pace.

Today, there are several key trends reshaping those requirements:

  • Equipment densification demands smarter design
    In a short period of time, GPU densities have skyrocketed. Where early deployments housed eight GPUs per cabinet, as many as 72 are in the same footprint today. Connectivity preferences are shifting, too, with more MPO8 APC connectors at the GPUs and CPUs, multimode fiber within cabinet rows and singlemode fiber reaching beyond the rows via double-density transceivers that provide 16 fibers per port. As cable and connection designs become more robust, cable management becomes a top priority.

    However, equipment rooms are running out of space as more power and cooling equipment are needed to support more servers. The space constraints in data centers require modular fiber frames that provide shallower footprints and flexible deployment options – wall-mount, side-by-side, back-to-back – to maximize square footage and simplify installation.

  • Faster refresh cycles require modular speed
    Driven by advances in chipsets, electronics refresh cycles have shrunk from five years to three years (with 12-month lifecycles now common). Fiber frames must adapt to increasing densities, offer more breakout configurations and reduce the time needed to connect and turn up the new gear.

    Modular and repeatable components such as panels, cassettes and adapter packs, enable offsite pre-building and pre-loading of the frames, which can then roll in ready to connect, further reducing the time needed for equipment refreshes and turn up services. Fiber frame agility isn’t just a technical benefit, it also offers a financial and business advantage. Faster deployments reduce labor hours and planned downtime, delivering significant real savings as AI infrastructure costs continue to climb.

  • Simplified systems for a de-skilled workforce
    As AI-ready data centers expand, the existing pool of skilled technicians is struggling to keep up with the growth. This emphasizes the need for simplified network systems that are more intuitive and simpler to deploy, adapt and maintain. Modular fiber frames enable less-experienced techs to quickly expand or reconfigure capacity using interchangeable plug-and-play cassettes and adapter packs. And QR-coded components offer instant access to tutorials for new techs, reducing errors and training time.

    On the macro level, data centers can achieve even more efficiency and flexibility with a standardized and modular fiber delivery platform. These integrated ecosystems include modular cable assemblies, connectors, frames, panels and components designed to work together across all areas of the data center. With one modular system, techs can manage fiber delivery anywhere in the data center with one set of components instead of mastering multiple systems and solutions. A unified ecosystem also ensures a coordinated roadmap for system additions and enhancements as data center refresh rates accelerate.

  • Fiber frames: Built for AI-Ready Infrastructure
    As demand for AI applications mushrooms, there is mounting pressure on data centers to adapt. Next-generation fiber frames that are more modular, streamlined and agile can help.



Commscope Hero

Discover how we can help transform your data center with modular fiber frames.


 

ABOUT THE SPONSOR

This article was brought to you in partnership with Commscope.
Now meets next. CommScope pushes the boundaries of communications technology to create the world’s most advanced networks. They design, manufacture, install, and support the hardware infrastructure and software intelligence that enable our digital society to interact and thrive. Working with customers, CommScope advances broadband, enterprise, and wireless networks to power progress and create lasting connections. Across the globe, CommScope’s people and solutions are redefining connectivity, solving today’s challenges, and driving the innovation that will meet the needs of what’s next.



You might also like