Data center managers with tablet



SPONSORED

Smart Surveillance for Modern Data Centers: Securing Our Digital World


Think about the disruption caused by cell phone outages, Wi-Fi failures and large-scale data breaches. These incidents can bring both business and personal activities to a standstill. At the heart of our digital-first world are data centers, where specialized facilities house the servers, networking equipment and computer systems that power everything from cloud connectivity to critical infrastructure.

With the global data center market projected to reach $452.5 billion in 2025 – up from $344 billion in 2024 – and continue growing at 8.4 percent annually through 2029, the market’s impressive numbers present ample opportunity for industry professionals.1 But that growth comes with a catch: a constantly evolving array of security challenges.

The Evolving Landscape of Data Center Security

With the rapid expansion of data centers comes a new set of security challenges. Today’s facilities face not only traditional physical threats but also progressively more sophisticated cyber and compliance risks. Security professionals and data center managers are seeking solutions that can adapt to evolving threats, ensure uptime and meet stringent regulatory requirements.

With these shifting strategic imperatives, data center operators are increasingly looking to partner with technology providers who can guide them through these complexities while considering their unique needs and requirements. Working with the right partner, with the right product design approach to meet data centers’ needs, is the foundation for building an integrated, intelligent security architecture. This ensures a center is fully protected, from server racks to the perimeter fence line, while also supporting corporate goals and compliance standards.

Getting Smarter About Data Center Surveillance

Data center managers are employing artificial intelligence (AI), advanced analytics and thermal imaging technologies to bolster their surveillance posture and minimize threat surfaces.

AI Surveillance for Data Centers

Unauthorized physical access is a major issue, especially “tailgating,” which is when an unauthorized person follows an authorized user through a secure entry. AI-powered surveillance cameras can detect if more than one person gains access on a single credential swipe, alerting staff to potential breaches. This proactive approach helps prevent tailgating incidents and strengthens perimeter protection.

Bandwidth and Storage Optimization

With thousands of high-resolution video streams running simultaneously, data centers risk bandwidth overload and escalating storage costs without intelligent compression and accurate classification tools.

Hanwha Vision cameras use AI and deep learning algorithms to detect and classify distinct objects (people, vehicles, faces and license plates) while clearly distinguishing them from their environmental surroundings. By focusing only on relevant activity and filtering out visual noise, data centers can significantly reduce their number of false alarms and lower bandwidth usage by as much as 80% while maintaining, or even improving, situational awareness.

Thermal Cameras: From Security to Preventative Maintenance

Thermal imaging is now a core component of modern data center security and facility management. Hanwha Vision’s bi-spectrum thermal cameras provide real-time visualization of heat flow, enabling detection of environmental anomalies, hotspots or leaks in liquid cooling systems.

Key Applications:

  • Campus Security – Thermal cameras can secure high-risk zones like loading docks, staff ingress/egress points, fuel storage systems and rooftops as a non-intrusive method of detecting heat signatures and movement, even in complete darkness.
  • Preventative Maintenance – Radiometric thermal cameras with dual-spectrum capabilities can identify subtle temperature anomalies over time. For example, if a server rack operates 20 percent hotter than usual, it could signal a power supply issue before failure occurs. This technology also helps confirm proper air and fluid flow in high-density, liquid-cooled environments.

Increasingly, data centers are strengthening their physical perimeter security in response to stricter service level agreement (SLA) requirements from enterprise clients and to qualify for government contracts. For instance, Department of Defense bids now emphasize that data centers have an installed and active perimeter monitoring system, making robust perimeter protection a critical factor for compliance and business growth.

Despite the importance of perimeter security as the first line of defense for data centers, fewer than 10% of data centers currently employ active perimeter protection.2 To secure these critical access points, AI analytics can be used to recognize suspicious activity, such as a person walking along a fence line, and trigger alerts well before a breach occurs, moving security from reactive to proactive.

Compliance and Scalability: Built for the Data Center Environment

In an industry where uptime is paramount, supply chain reliability and compliance are non-negotiable. Hanwha Vision’s approach begins at the source of global manufacturing and security: the factory.

  • End-to-End Manufacturing – Hanwha Vision owns the entire manufacturing process, building its Wisenet System on a Chip (SoC) in-house. Each chip includes embedded certificates and encryption keys, and each device has a built-in Trusted Platform Module (TPM), simplifying compliance with strict internal audits and cybersecurity requirements.
  • Regulatory Assurance – Hanwha Vision surveillance equipment is NDAA-compliant and meets FIPS-140-3 security standards, ensuring freedom from questionable third-party firmware or components.
  • Operational Efficiency – Advanced surveillance platforms like Hanwha Vision’s Wisenet SoC feature dual Neural Processing Units and intelligent compression algorithms, reducing storage and network strain without sacrificing image quality. Eco mode allows cameras to operate on low power, supporting sustainability goals and conserving energy while still providing essential functionality.

Trusted Partners for Management and Integration

For large-scale facilities, cloud security systems and video management platforms are transforming how data centers monitor and respond to threats. These solutions enable centralized control, rapid deployment and seamless integration with existing infrastructure.

This level of development expertise goes hand-in-hand with the approach of being a true partner to customers. Being easy to work with is as important as product specs. Ultimately, protecting a data center comes down to trust, relationships, reliability and enabling smarter operations in one of the world’s most complex and critical environments. Finding a partner with expertise in deployment and integration ensures that data center managers can scale their surveillance systems efficiently and reliably.




Data center

Learn more about how Wesco can help you upgrade your data center security.



 

ABOUT THE SPONSOR

This article was brought to you in partnership with Hanwha Vision.
Hanwha Vision offers a mix of devices and software that combine optical design expertise and image processing innovation with 24/7 protection, artificial intelligence, analytics and cloud-based management. With IP cameras, storage devices, video management software, recorders, encoders/decoders, monitors and accessories, Hanwha Vision designs and builds the surveillance technology solutions customers need to protect their operations today and keep their businesses moving forward.


You might also like